How open-source software is driving the adoption of standards in EV charging

What open-source software means for EV charging, interoperability and the EV market

21 OCT 2024 | Technology and innovation

With projections that the number of electric vehicles (EVs) will represent more than 60% of global vehicle sales by 2030, the number of EV chargers must grow proportionally. There is a clear need for a reliable EV charging infrastructure; however, inconsistency among EV charger connectors, plug types and charging protocols can increase range anxiety and even influence drivers’ purchasing decisions, because they are unsure whether the vehicle they’re considering will be compatible with the chargers they’ll need on local or long-distance trips.

To address the concerns of EV drivers and simplify the charging experience, the answer seems simple: employ EV charging standards for charging stations that enable compatibility between almost any EV and the grid, also known as interoperability.

“Standards are important so that cars can communicate across common protocols and interfaces to EV chargers, and so that EV chargers have standardized interfaces to communicate back to utilities,” said Henrik Mannesson, general manager of energy infrastructure at our company.

“Being able to charge your EV and not having to worry about having the right adapter or connector is super important to the success of the energy transition and EV charging,” said Brandon Kanter, systems manager of EV charging.

Because there are many EV manufacturers and charger types, the road to standardization is complex. Standardization efforts require both software and hardware, and open-source software in particular is especially crucial. Given its accessibility and collaboration-focused nature, open-source software has the potential to address interoperability challenges.

Open-source software, standardization and market growth

Open-source software is a collection of software stacks, or collections of code, that enable a device or system such as an EV charger to implement an action, like charging communication. Anyone can access and contribute to open-source software code, which gives it particular advantages and benefits in the context of standards.

At events called plugfests, design engineers test compatibility with their stacks and various EVs; the best software stacks can become standardized. “The stack becomes the standard because everyone tested and gave feedback and came to an agreement. Now we can all take this software stack and use it,” said Artem Aginskiy, general manager of Arm®-based processors.

The accessibility and collaborative nature of open-source software benefits EV charging manufacturers in several ways. With a standardized stack, EV charger manufacturers can alleviate interoperability challenges. Charger manufacturers benefit from faster time to market and lower development costs because open-source software is so accessible. Manufacturers can meet the demand for an expanded EV charging infrastructure. System reliability improves as well; because several people review the same code and find bugs, finding and resolving issues within software happens more quickly.

For EV owners, not only does standardized software make their driving and charging experience easier, they can also look forward to more long-term support. In other words, since anyone can contribute to open-source software, EV owners don’t have to worry about their charging experience changing if one EV charger manufacturer discontinues their product. The improved reliability and uniformity of charging has the potential to increase driver confidence and proliferate EV adoption.

And by having visibility into charger source code (and the protocol implementations within that code), EV manufacturers can check that their proprietary (closed-source) solutions remain compatible with the charging infrastructure implemented on the other end of the vehicle.

How TI has embraced open source

The transition to open-source software is one that our company has embraced, both by supporting the development and adoption of standards, and by providing a wide range of EV charging-related reference designs.

The standardization of open-source software allows for further optimization of hardware. “Our Arm-based processors run standard Linux distributions, making it easy for manufacturers to integrate our hardware into their charging systems,” Brandon said. Our processors also support the addition of wired and wireless connectivity devices across various protocols, depending on the need for that charger.

Our company’s support goes beyond hardware; we also provide direct support for the development of software. “We’ve worked with third parties to develop an electric vehicle service equipment kit, an EV charging reference design that designers can use to implement EV supply equipment,” Artem said.

We’ve also engaged with third parties by hosting events for the open-source community. Our upstream-first mentality means providing support to third parties adopting open source before a device is widely available, so they can review code for a certain standard in advance. This enables them to start working quickly and remove potential software driver barriers.

Open source and the future

As more EV charging companies adopt and build upon open-source technology, EV charging networks have the potential to achieve new feats in interoperability with the grid.

“There are two sides to a charging station – the EV side, and the side that’s drawing power from the local electric utility,” Henrik said. “You want the connection on both sides to be seamless so that the charging station can talk back and forth with the utilities.”

EV interoperability is an important part of that vision. By sharing data in a standardized way, the grid can better adapt and shed demand, relieve stress on the grid, or increase capacity. Even at the residential level, industry standards achieved through open source enable the use of bidirectional charging to intelligently shed load from the grid to prevent it from overloading. This means that charged EVs may be able to send electricity to the grid when prices are high, and consume electricity from the grid when prices are low.

Advancements that open source enables have the potential to bolster the growth of EV ownership, increase consumer confidence in the reliability and accessibility of chargers and the charging experience and build out a much-needed EV charging infrastructure.

“Agreeing about how the different pieces are connected isn’t just a positive for TI; it’s a positive for consumers, and essential to EV industry growth and sustainability,” Brandon said. “Everybody’s contributing, and we are proud to play an important role.”

Related company blog posts

Why packaging is the next frontier in power design innovation
23 Mar 2026 | Technology and innovation
Why packaging is the next frontier in power design innovation

As power systems demand more capability within fixed areas, packaging innovations enable greater integration, safety and performance

3 semiconductor technologies that are redefining the EV experience
16 Mar 2026 | Technology and innovation
3 semiconductor technologies that are redefining the EV experience

How collaboration-driven semiconductor technologies are transforming EVs into a practical, everyday option

Beyond sound: How semiconductor innovation is transforming audio experiences
20 Feb 2026 | Technology and innovation
Beyond sound: How semiconductor innovation is transforming audio experiences

Audio makes our lives richer, more personal, and even safer. When you add semiconductors, what’s possible?

View all
Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.