Imprivata® and TI to deliver embedded strong authentication for thin- and zero-client devices in the healthcare industry

Integrated No Click Access™ on TI's DM8148 system-on-chip to create standard for authentication in virtual desktop environments

27 SEP 2012 | Uncategorized

LEXINGTON, Mass. and DALLAS, Sept. 27, 2012 /PRNewswire/ --  Imprivata, the leader in healthcare IT security, and Texas Instruments Incorporated (TI) (NASDAQ: TXN) today announced a collaboration to support strong authentication and secure application access from virtual desktop environments. The solution, combining TI's DM8148 system-on-chip (SoC) and Imprivata OneSign will enable manufacturers to provide out-of-the-box strong user authentication into any software application delivered via a thin- or zero-client endpoint. This type of integrated technology is particularly attractive in healthcare, where highly mobile care providers need fast, secure access to sensitive patient information on shared devices, and IT teams strive to lower maintenance and increase security by centralizing data. 

TI's DM8148 SoC: Driving leading-edge virtual desktop capabilities 
With the ability to deliver high performance at low power levels, TI's cost-effective DM8148 SoC drives optimized virtual desktop capabilities in a power efficient, secure manner. The SoC's intelligent architecture includes a programmable DSP to accelerate virtual desktop protocols and on-chip HD video accelerators for rich multimedia experiences, including 1080p video streaming. The DM8148 supports dual-displays (cloned or extended desktop) running concurrently up to 1920x1200 (WUXGA) resolution, and supports the leading Virtual Desktop Infrastructure (VDI) protocols for ultimate flexibility.  The low-power SoC enables OEMs to create a fanless design, which yields greater reliability and lower maintenance for thin-client systems. 

To fully utilize the capabilities of the DM8148 SoC, TI also developed a software reference design kit (RDK) for thin and zero clients.  Through its partnership with TI, Imprivata enables thin- and zero-client vendors to embed Imprivata OneSign strong authentication functionality directly into their devices incorporating the TI DM8148 SoC. This solution allows manufacturers to simplify their development and ensure Imprivata Ready accreditation for their products. The DM8148 SoC and the DM8148 software RDK are available today. Click here for more details.

Imprivata OneSign: The standard for secure clinical authentication on virtual desktops
Imprivata OneSign enables strong authentication across a wide range of operating systems, applications and devices with the broadest support of authentication modalities, including fingerprint biometrics, proximity and smart cards, one-time passwords, and USB tokens. Through the Imprivata Developer Program (IDP), Imprivata enables third-parties to integrate OneSign authentication into software and hardware via a family of application programming interfaces (API) and software called OneSign ProveID™.  Imprivata OneSign ProveID Embedded is a software layer that supports TI's DM8148 SoC and RDK, and is directly integrated within thin- and zero-client solutions to provide native authentication. In addition to supporting fast and secure data access, OneSign provides manufacturers and end users with flexibility, along with reassurance that technology investments will provide long-term value and simplified management. With desktop virtualization adoption in hospitals expected to grow by 44% in 2013[1], Imprivata OneSign strong authentication allows users to benefit from No Click Access, which is essential for care providers who need instant access to protected clinical data.

"In healthcare, there is little delineation between the public and private spaces in which clinicians work, and care providers are constantly accessing patient information across shared workstations throughout a hospital. This poses a unique workflow and security challenge," said David Ting, founder and chief technology officer at Imprivata. "Desktop virtualization, when coupled with No Click Access, provides clinicians with fast, secure access to patient information, regardless of location. Used by over 2 million healthcare providers worldwide, Imprivata OneSign has become the standard for access and authentication in healthcare. Combined with TI's unparalleled technologies, Imprivata OneSign provides healthcare providers with strong authentication across more devices and operating environments than any other vendor in the industry."

"As interest in desktop virtualization continues to grow, the need for strong authentication and single sign-on also continues to rise," said Kim Devlin-Allen, thin client business manager, OMAP™ platform business unit, TI. "Meeting this demand, TI's DM8148 offers leading-edge performance and power advantages to enable cost-effective thin and zero clients, particularly in the highly regulated healthcare market. We are excited about the opportunity to showcase the DM8148 RDK software optimized with Imprivata's strong authentication technology, and to pave the way for new advancements in the embedded thin- and zero-client markets."

"Thin client desktop virtualization is a fast-growing trend in healthcare, as IT staff and clinical users look to reduce maintenance, secure end points and speed clinical workflows," commented Judy Hanover, IDC Health Insights research director. "Integrating strong authentication with SoC technology provides an attractive solution for end-to-end security, while also giving care providers fast and easy access to critical applications."

About Texas Instruments
Texas Instruments semiconductor innovations help 90,000 customers unlock the possibilities of the world as it could be – smarter, safer, greener, healthier and more fun. Our commitment to building a better future is ingrained in everything we do – from the responsible manufacturing of our semiconductors, to caring for our employees, to giving back inside our communities. This is just the beginning of our story. Learn more at www.ti.com.

About Imprivata
With nearly 3 million users and 1,300 healthcare customers, Imprivata is the #1 provider of secure access solutions for healthcare. By strengthening user authentication, streamlining application access and simplifying compliance reporting across multiple computing environments, customers realize improved workflows, increased security and compliance with government regulations.

Imprivata has received numerous product awards and top review ratings from leading industry publications and analysts, including a Strong Positive rating in Gartner's 2011 Marketscope for ESSO, the #1 ranking in the KLAS SSO Performance report and the #1 rating in 2010 Best in KLAS and Category Leaders report. Headquartered in Lexington, Mass., Imprivata partners with over 200 resellers, and serves the access security needs of customers around the world. For more information, please visit www.imprivata.com or follow us on Twitter at @Imprivata.

Follow Imprivata on Twitter: https://twitter.com/Imprivata
Like Imprivata's Facebook Page: www.facebook.com/Imprivata
Connect with Imprivata on LinkedIn: www.linkedin.com/company/imprivata

Trademarks
All Imprivata products are trademarks of Imprivata, Inc. in the USA and other countries. OMAP is a trademark of Texas Instruments. All other product or company names mentioned are the property of their respective owners.

[1] 2012 Desktop Virtualization Trends in Healthcare Research Report, Imprivata, August 2012

SOURCE Texas Instruments Incorporated; Imprivata

Related news releases

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming
27 Jul 2021 | Uncategorized

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming

Available for back to school, the newest TI graphing calculator brings popular Python programming language to the classroom

View all

Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.