TI unveils first ultra-low power dual-band wireless MCU in production

Monitor IoT networks from a handheld device with TI's single-chip Sub-1 GHz and Bluetooth® low energy solution available today

14 SEP 2016 | Uncategorized

DALLAS, Sept. 14, 2016 /PRNewswire/ -- Expanding the functionality of Internet of Things (IoT) networks, Texas Instruments (TI) (NASDAQ: TXN) today announced availability for mass production of the industry's lowest-power dual-band wireless microcontroller (MCU) supporting Sub-1 GHz and Bluetooth® low energy connectivity on a single chip. As part of TI's pin-to-pin and software compatible SimpleLink™ ultra-low power platform, the new SimpleLink dual-band CC1350 wireless MCU enables developers to move from a three-chip solution to a tiny single chip, while reducing design complexity, saving power, cost and board space. The CC1350 wireless MCU offers a range of up to 20 km on a coin cell battery for building and factory automation, alarm and security, smart grid, asset tracking and wireless sensor network applications. For more information, visit www.ti.com/cc1350-pr.

Experience the interactive Multimedia News Release here: https://www.multivu.com/players/English/7746254-texas-instruments-simplelink-dual-band-cc1350

Tune into our virtual press conference today, September 14 at 9:00 a.m. CST on Facebook Live to learn more.

Designed for low-power wide area networks (LPWAN), the CC1350 wireless MCU features:

  • Dual-band connectivity that expands the functionality of a Sub-1 GHz network with Bluetooth low energy implementations such as beaconing, over-the-air updates, smart commissioning, remote displays and more.
  • Long-range connectivity paired with ultra-low power consumption that offers a sleep current of 0.7 uA which allows for more than 10 years of battery life.
  • Enhanced integration in a tiny wireless MCU that combines a Sub-1 GHz transceiver and Bluetooth low energy radio, as well as an ARM® Cortex®-M3 core in a single, Flash-based, 4x4 mm QFN package.

Developers can get started in minutes with the low-cost SimpleLink CC1350 wireless MCU LaunchPad™ development kit or connect sensors to the cloud in minutes with the SimpleLink CC1350 SensorTag demo kit supported by TI's Code Composer Studio™ integrated development environment (IDE) and IAR Embedded WorkBench®. Additionally, TI has simplified development by providing multiple software options including point-to-point communication examples with EasyLink, a wireless M-Bus protocol stack leveraging TI RTOS, as well as the BLE-Stack 2.2 software development kit (SDK) which supports Bluetooth 4.2 specifications. Developers will also have access to online training and E2E™ community support to help ease their design process.

Pricing and availability
SimpleLink Sub-1 GHz CC1350 wireless MCU-based development kits are available now on the TI Store and through TI authorized distributors.

  • CC1350 LaunchPad kit (LAUNCHXL-CC1350): USD $29.00 – develop a complete prototype with a low-cost Sub-1 GHz and Bluetooth low energy wireless MCU hardware, software and RF development platform.
  • CC1350 SensorTag demo kit (CC1350STK) coming in 4Q 2016: $29.99 – demonstrate your Sub-1 GHz and Bluetooth low energy project with a small, sensor-based kit which includes 10 low-power MEMS sensors and can connect to the cloud in less than three minutes.

The SimpleLink Sub-1 GHz CC1350 wireless MCUs, for operation in 315 MHz, 433 MHz, 470 MHz, 500 MHz, 779 MHz, 868 MHz, 915 MHz and 920 MHz and 2.4 GHz ISM bands and SRD systems, will be available in 4x4, 5x5 and 7x7 mm QFN packages. The devices available today are for 868 MHz, 915 MHz and 920 MHz ISM band operation and the 7x7 mm pricing is as follows:

  • CC1350F128RGZR: $4.60 in 1,000 unit volumes

Learn more about TI's SimpleLink ultra-low power platform:

  • Discover the benefits of TI's ultra-low power wireless MCUs.
  • Learn more about advantages of Sub-1 GHz and Bluetooth low energy in a single chip in this white paper.
  • Watch the why Sub-1 GHz + Bluetooth low energy video.
  • Read more about CC1350 wireless MCUs on the ConnecTIng Wirelessly blog.

TI's SimpleLink wireless connectivity portfolio
TI's SimpleLink portfolio of low and ultra-low power wireless connectivity solutions – wireless MCUs and wireless network processors (WNPs) for the broad embedded market – makes it easier to develop and connect anything to the Internet of Things (IoT). Spanning over 14 standards and technologies including Bluetooth ® Smart, Wi-Fi®, Sub-1 GHz, 6LoWPAN, Thread, ZigBee® and more, SimpleLink products help manufacturers easily add wireless connectivity to anything, to any design, for anyone. www.ti.com/simplelink.

About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog ICs and embedded processors. By employing the world's brightest minds, TI creates innovations that shape the future of technology. TI is helping more than 100,000 customers transform the future, today. Learn more at www.ti.com.

Trademarks
SimpleLink, Code Composer Studio and E2E community are trademarks of Texas Instruments. All other trademarks belong to their respective owners.

Save power and space with the new CC1350 wireless MCU from TI

 

The SimpleLink™ dual-band CC1350 wireless MCU for Sub-1 GHz and Bluetooth low energy connectivity on a single chip

 

The SimpleLink dual-band CC1350 wireless MCU integrates a Sub-1 GHz transceiver, Bluetooth low energy radio and an ARM Cortex-M3 core in a tiny 4x4mm chip.

 

To view the original version on PR Newswire, visit:http://www.prnewswire.com/news-releases/ti-unveils-first-ultra-low-power-dual-band-wireless-mcu-in-production-300327165.html

SOURCE Texas Instruments

Related news releases

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming
27 Jul 2021 | Uncategorized

Texas Instruments new TI-84 Plus CE Python graphing calculator introduces students to programming

Available for back to school, the newest TI graphing calculator brings popular Python programming language to the classroom

View all

Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.