New TI MCUs enable edge AI and industry-leading real-time control to advance system efficiency, safety and sustainability
News highlights:
- The new TMS320F28P55x series of C2000™ MCUs with an integrated edge artificial intelligence (AI) hardware accelerator enables smarter real-time control, with up to 99% fault detection accuracy.
- The latest 64-bit C29 core in the new F29H85x series more than doubles the real-time control performance of existing generations and will have an integrity level up to Automotive Safety Integrity Level (ASIL) D and SIL 3.
DALLAS, Nov. 11, 2024 /PRNewswire/ -- Texas Instruments (TI) (Nasdaq: TXN) today introduced two new series of real-time microcontrollers that deliver advancements to help engineers achieve more intelligent and secure processing in automotive and industrial applications. TI's TMS320F28P55x series of C2000™ MCUs is the industry's first portfolio of real-time microcontrollers with an integrated neural processing unit (NPU), enabling fault detections with high accuracy and low latency. The F29H85x series is built on TI's new 64-bit C29 digital signal processor core and offers an advanced architecture with integrated safety and security features. TI will display both devices at electronica 2024, Nov. 12-15, in Munich, Germany.
For more information, see ti.com/TMS320F28P550SJ, ti.com/TMS320F28P559SJ-Q1, ti.com/F29H850TU, and ti.com/F29H859TU-Q1.
"Engineers increasingly strive to design automotive and industrial applications that are more energy efficient and can make faster decisions, driving a need for more scalable processing power, expanded memory, and on-chip safety and security enablers," said Amichai Ron, senior vice president, TI Embedded Processing. "For decades, our C2000 MCUs have been enabling manufacturers to measure and efficiently process real-world data. Today's introduction of enhanced real-time performance and edge AI in our C2000 portfolio will empower engineers to solve more complex problems and reach higher levels of system efficiency, safety and sustainability."
Empowering smarter, more efficient systems through edge AI-enabled MCUs
Engineers today are challenged to design systems that can make accurate, intelligent decisions in real time to perform functions such as arc fault detection in solar and energy storage systems and motor-bearing fault detection for predictive maintenance. As the industry's first real-time MCUs with an integrated neural processing unit, TI's new C2000™ TMS320F28P55x series meets both of these challenges by ensuring consistent performance with real-time processing.
The NPU in the TMS320F28P55x series offloads the execution of the neural network model from the main CPU, achieving five to 10 times lower latency than software implementations to enable faster, more accurate decision-making. Further, the model that runs on the integrated NPU learns and adapts to different environments through training, helping systems achieve greater than 99% fault detection accuracy to enable more informed decision-making at the edge. TI's complete AI toolchain, which includes models that are optimized and tested for specific applications, helps engineers with any level of experience easily complete the AI model development process.
To learn more about AI-enabled real-time control applications, read the technical article, "Optimizing system fault detection in real-time control systems with edge AI-enabled MCUs."
Enabling industry-leading real-time control performance with advanced safety and security
Designers are increasingly looking for a single MCU with more flash memory, larger computational capabilities and more integrated functionality. This need is particularly evident as vehicles shift from discrete solutions to integrated solutions, where a single chip is capable of handling various computational and housekeeping functions within the powertrain. TI's new C29 core, with its 64-bit architecture, delivers more than double the real-time signal-chain performance of the C28 core.
Featuring comprehensive diagnostics and error-checking mechanisms, the F29H85x series was engineered for compliance with International Organization for Standardization 26262 and International Electrotechnical Commission 61508 automotive and industrial safety standards, with levels up to ASIL D and SIL 3. These MCUs also provide cybersecurity capabilities, with a fully isolated hardware security module that protects systems from unauthorized access and cyberthreats. Additionally, TI's proprietary safety and security unit provides runtime safety and security without a performance penalty using an advanced, context-aware memory protection unit for hardware isolation of CPU tasks, with freedom from interference and self-test processes.
To learn more about how TI helps engineers solve processing and safety design challenges, read the article, "How MCUs Built With Innovative C29 Cores Increase Real-Time Performance in High-Voltage Systems."
TI at electronica 2024
At electronica 2024, TI will showcase how its analog and embedded processing products are helping design a more intelligent and sustainable future. Demonstrations include the latest advancements in robotics, industrial communications, edge AI and intelligent systems, energy infrastructure, and software-defined vehicles. See ti.com/electronica for more information.
Highlights during the show include:
- Tuesday, Nov. 12-Friday, Nov. 15: Visit TI in the Neue Messe München exhibition center, hall C4, booth 159.
- Tuesday, Nov. 12:
- Chen Yu Chang presents "Reinventing Real-Time Control with Advanced CPU Architecture."
- Ibukun Olumuyiwa presents "Enabling Cybersecurity for High-Performance Real-Time Microcontrollers."
- Wednesday, Nov. 13:
- Arthur Redfern participates in "Embedded AI: Bridging the Gap from High-Level Neural Network Design to Low-Level Embedded Execution."
- Friday, Nov. 15:
- Daolin Qiu and Pekka Varis present "Network Redundancy for Smart Grid Performance Measurements."
Package, availability and pricing
- The TMS320F28P550SJ and TMS320F28P559SJ-Q1 are available now at ti.com/C2000 in preproduction quantities, with the F29H850TU and F29H859TU-Q1 available by year-end 2024.
- Multiple payment and shipping options are available.
- Includes evaluation modules.
About Texas Instruments
Texas Instruments Incorporated (Nasdaq: TXN) is a global semiconductor company that designs, manufactures and sells analog and embedded processing chips for markets such as industrial, automotive, personal electronics, communications equipment and enterprise systems. At our core, we have a passion to create a better world by making electronics more affordable through semiconductors. This passion is alive today as each generation of innovation builds upon the last to make our technology more reliable, more affordable and lower power, making it possible for semiconductors to go into electronics everywhere. Learn more at TI.com.
Trademarks
C2000 is a trademark of Texas Instruments. All registered trademarks and other trademarks belong to their respective owners.
SOURCE Texas Instruments