TI’s new programmable logic portfolio helps engineers go from concept to prototype in minutes

New programmable logic devices and no-code design tool reduce engineering design complexity, board space, time and costs

10 OCT 2024 | Products and technologies

TI’s new programmable logic portfolio allows engineers to integrate up to 40 logic and analog functions on a single chip, drastically reducing board size compared to discrete implementation. 

What’s new

Building on its industry-leading logic portfolio, Texas Instruments (TI) today introduced programmable logic devices (PLDs) that empower engineers to streamline their logic designs for any application. With the ability to integrate up to 40 combinational and sequential logic and analog functions into one device, TI’s new PLD portfolio can help reduce board size as much as 94% - and lower system costs - compared to discrete logic implementations. Moreover, the new portfolio offers significant space savings compared to similar programmable logic devices on the market.

Leveraging TI’s easy-to-use InterConnect Studio tool, engineers can design, simulate and configure their devices for evaluation in minutes without the need for any software coding. InterConnect Studio expedites the logic design process with a drag-and-drop GUI and integrated simulation feature. Designers also benefit from click-to-program and direct ordering features that simplify programming and procurement, helping to accelerate time to market.

For more information, see ti.com/tpld.

Why it matters

“Engineers are increasingly considering programmable logic devices as a way to reduce design complexity and board space, simplify supply chain management, and accelerate their time to market,” said Tsedeniya Abraham, vice president and general manager of Interface at TI. “But existing programmable logic devices are more complex than many applications require, involve programming expertise, or they come in limited packaging options. Our new programmable logic portfolio builds on TI’s 60 years of experience in logic design and offers small form factors in industry-standard packaging as small as 2.56mm2, low power consumption, AEC Q-100 qualification and a temperature range of -40°C to 125°C for applications including automotive, industrial and personal electronics.”

To learn more, see the technical article, “Unlocking the possibilities of programmable logic.”

More details

TI's PLD portfolio includes the industry's smallest leaded package across all markets, measuring 2.1mm by 1.6mm with a 0.5mm pitch. This leaded package is 92% smaller than competing devices, supporting manufacturers’ need for solderability – at a fraction of the size. TI’s automotive-grade PLDs are as much as 63% smaller than their closest competitors. The portfolio also offers quad flat no-lead (QFN) packaging options that enable automated optical inspection, ensuring safety and long-term system reliability.

With quiescent current less than 1µA and 50% less active power than similar devices on the market, TI’s new PLDs offer low power consumption to help extend battery life in products such as electric vehicles, power tools, battery packs and gaming controllers.

All of TI’s new PLDs support general-purpose input/output, look-up tables, digital flip-flops, pipe delays, filters, and resistor-capacitor oscillators. The TPLD1201 and TPLD1202 devices also integrate analog functions such as analog comparators, with internal selectable voltage reference options and hysteresis. The TPLD1202 offers additional elements such as Serial Peripheral Interface, I2C, a watchdog timer and a state machine.

Availability

Preproduction quantities of TI’s new PLDs are available at TI.com. The table below provides details and pricing in 1,000-unit quantities. Additionally, development tools include:

  • Evaluation modules for purchase on TI.com for US$69.
  • A USB programmer for US$59.
  • InterConnect Studio, as a free download on TI.com.
Device
Package
Price 
Evaluation module
TPLD801 SOT – 8-pin US$0.19 TPLD801-DRL-EVM
TPLD801-Q1 SOT – 8-pin US$0.224 TPLD801-DRL-EVM
TPLD1201 VSSOP – 10-pin US$0.34 TPLD1201-DGS-EVM
QFN – 12-pin US$0.38 TPLD1201-RWB-EVM
TPLD1201-Q1 VSSOP – 10-pin US$0.40 TPLD1201-DGS-EVM
TPLD1202 SOT – 14-pin  US$0.44 TPLD1202-DYY-EVM
QFN – 12-pin US$0.48 TPLD1202-RWB-EVM
TPLD1202-Q1 SOT – 14-pin US$0.52 TPLD1202-DYY-EVM

About Texas Instruments

Texas Instruments Incorporated (Nasdaq: TXN) is a global semiconductor company that designs, manufactures and sells analog and embedded processing chips for markets such as industrial, automotive, personal electronics, communications equipment and enterprise systems. At our core, we have a passion to create a better world by making electronics more affordable through semiconductors. This passion is alive today as each generation of innovation builds upon the last to make our technology more reliable, more affordable and lower power, making it possible for semiconductors to go into electronics everywhere. Learn more at TI.com.

Related news releases

TI expands microcontroller portfolio and software ecosystem to enable edge AI in every device
10 Mar 2026 | Products and technologies

TI expands microcontroller portfolio and software ecosystem to enable edge AI in every device

New MCUs with the TinyEngine™ NPU join TI's comprehensive portfolio of AI-enabled hardware, software and tools, allowing engineers to deploy intelligence anywhere

TI accelerates the next generation of physical AI with NVIDIA
05 Mar 2026 | Products and technologies

TI accelerates the next generation of physical AI with NVIDIA

TI's real-time control, sensing and power portfolios combined with NVIDIA technology advance development of safer humanoid robots

TI accelerates the shift toward autonomous vehicles with expanded automotive portfolio
05 Jan 2026 | Products and technologies

TI accelerates the shift toward autonomous vehicles with expanded automotive portfolio

New analog and embedded processing technologies from TI enable automakers to deliver smarter, safer and more connected driving experiences across their entire vehicle fleet News highlights: TI's...

View all

Media contact

Reporters and editors can contact TI’s media relations team at: mediarelations@ti.com
To contact another group at TI, please visit the TI Contact Us page.