Visit TI at embedded world
11-13 March | Nuremberg, Germany
Hall 3A, Booth 131
TI at embedded world 2025
Reimagine embedded systems with edge AI and connectivity technologies
At home, in the car or on the job everywhere we go embedded technology is impacting our lives driving the need for semiconductors that are more intelligent, connected and smaller than ever before. With our scalable embedded portfolio and industry-standard software, transform your data at the edge into meaningful insights and transfer that data securely without interference in industrial, automotive and medical applications. Every connected device, every smarter decision, every intuitive solution enables developers to reimagine embedded systems helping create an intelligent and connected world.
Time | Location/Session | Session title | Speaker |
---|---|---|---|
13:30 | Conference Area NCC East | C-Level @ embedded world | Ahmad Bahai Ph.D. |
14:45 | NCC Ost Convention Centre | Network Traffic Tunneling on Heterogeneous SoCs | Nitika Verma |
Time | Location/Session | Session title | Speaker |
---|---|---|---|
15:30 | NCC Ost Convention Centre | Time Synchronization over Network Redundancy in Real-Time Applications | Daolin Qiu |
Time | Location/Session | Session title | Speaker |
---|---|---|---|
09:30 | NCC Ost Convention Centre | Audio Solutions with TSN - Architecture for Zonal Automotive ECUs | Nilabh Anand |
10:30 | NCC Ost Convention Centre | Boot Time Optimization for Early Display and Graphics in EmbeddedSystems | Divyansh Mittal |
12:15 | NCC Ost Convention Centre | Faster Time to Market, Effective mmWave Radar Prototyping: A UnifiedApproach with TI MMIC and MATLAB | Matthiew Chevrier, TI |
14:30 | NCC Ost Convention Centre | Benchmarking Network Startup Time for Security-enforced Industrial IoT Devices | Nilabh Anand |
Reimagine decision-making with edge AI
Come by the TI booth to see advancements in real-time monitoring and perception with edge artificial intelligence.
Read our latest blog from Amichai Ron, senior vice president of embedded processing at our company, on how edge AI enables embedded devices to use sensor data more efficiently and enhance our everyday experiences.
See the latest medical wearables from TI with edge AI capabilities for detecting vital signs and classifying health insights. An on-chip neural processing unit delivers immediate and precise detection of cardiac events, allowing for early intervention or preventative care, while extending battery life.
Showcasing MCUs with edge AI capabilities for arc fault detection in solar energy systems. A dedicated hardware accelerator offloads the execution of the neural-network model from the main CPU, allowing enough computational and processing bandwidth to be reserved for high-accuracy, low-latency arc fault detection.
Reimagine IoT with scalable, secure connections
Support multiple wireless networks with one unified connectivity protocol, allowing for seamless, smart building automation. Visit our booth at embedded world to see how.
This demonstration shows how TI’s wireless connectivity portfolio, such as Bluetooth® Low Energy, Matter, Thread, Wi-Fi® and Zigbee®, support all smart building needs. Interact with different applications, such as connected lights, door locks, smart hubs and more, to see how different wireless technologies can fit within the same environment.
TI will highlight its certified, production-ready hardware and software for industrial communications using PROFINET®, EtherCAT® and EtherNet/IP™ software stacks. See how the technology enables seamless connectivity and real-time deterministic motor control with a single chip and licensed software for multi-protocol industrial Ethernet and Time Sensitive Networking over single-pair Ethernet.
Reimagine development with no-code tools and open-source software
Join us at our booth to explore a graphical development environment that enables users to configure, develop and run microcontroller applications in minutes with no coding or integrated development environment (IDE) required.