SBAS457F October 2010 – September 2019 ADS1118
PRODUCTION DATA.
If Config Register data are not required to be readback, the ADS1118 conversion data can also be clocked out in a short 16-bit data transmission cycle, as shown in Figure 42. Therefore, CS must be taken high after the 16th SCLK cycle. Taking CS high resets the SPI interface. The next time CS is taken low, data transmission starts with the currently buffered conversion result on the first SCLK rising edge. If DOUT/DRDY is low when data retrieval starts, the conversion buffer is already updated with a new result. Otherwise, if DOUT/DRDY is high, the same result from the previous data transmission cycle is read.