SBAS683B August 2014 – May 2020 ADS1120-Q1
PRODUCTION DATA.
To minimize leakage currents on the analog inputs, leave any unused analog and reference inputs floating, or connect the inputs to mid-supply or to AVDD. AIN3/REFN1 is an exception. Leave the AIN3/REFN1 pin floating when not used to avoid accidently shorting the pin to AVSS through the internal low-side switch. Connecting any unused analog or reference inputs to AVSS is possible as well, but can yield higher leakage currents than the previously mentioned options.
Do not float unused digital inputs; excessive power-supply leakage current can result. Tie all unused digital inputs to the appropriate levels, DVDD or DGND, even when in power-down mode. If CS is not used, tie this pin to DGND. If the internal oscillator is used, tie the CLK pin to DGND. If the DRDY output is not used, leave the pin unconnected or tie the pin to DVDD using a weak pullup resistor.