SBAS301D October 2003 – February 2020 ADS1204
PRODUCTION DATA.
The analog signal connected to the input of the ΔΣ modulator is converted using the clock signal applied to the modulator. The result of the conversion, or modulation, is generated and sent to the OUTx pin from the ΔΣ modulator. In most applications where a direct connection is realized between the ΔΣ modulator and an ASIC or FPGA (each with an implemented filter), the two standard signals per modulator (CLKOUT and OUTx) are provided from the modulator. The output clock signal is equal for all four modulators. If CLKSEL = 1, CLKIN must always be set either high or low.