SBAS752B May 2017 – October 2018 ADS122U04
PRODUCTION DATA.
The circuit in Figure 79 employs a ratiometric measurement approach. In other words, the sensor signal (that is, the voltage across the RTD in this case) and the reference voltage for the ADC are derived from the same excitation source. Therefore, errors resulting from temperature drift or noise of the excitation source cancel out because these errors are common to both the sensor signal and the reference.
In order to implement a ratiometric 3-wire RTD measurement using the device, IDAC1 is routed to one of the leads of the RTD and IDAC2 is routed to the second RTD lead. Both currents have the same value, which is programmable by the IDAC[2:0] bits in the configuration register. The design of the device ensures that both IDAC values are closely matched, even across temperature. The sum of both currents flows through a precision, low-drift reference resistor, RREF. The voltage, VREF, generated across the reference resistor (as shown in Equation 11) is used as the ADC reference voltage. Equation 11 reduces to Equation 12 because IIDAC1 = IIDAC2.
To simplify the following discussion, the individual lead resistance values of the RTD (RLEADx) are set to zero. As Equation 13 shows, only IDAC1 excites the RTD to produce a voltage (VRTD) proportional to the temperature-dependent RTD value and the IDAC1 value.
The device internally amplifies the voltage across the RTD using the PGA and compares the resulting voltage against the reference voltage to produce a digital output code proportional to Equation 14 through Equation 16:
As shown in Equation 16, the output code only depends on the value of the RTD, the PGA gain, and the reference resistor (RREF), but not on the IDAC1 value. The absolute accuracy and temperature drift of the excitation current therefore does not matter. However, because the value of the reference resistor directly affects the measurement result, choosing a reference resistor with a very low temperature coefficient is important to limit errors introduced by the temperature drift of RREF.
The second IDAC2 is used to compensate for errors introduced by the voltage drop across the lead resistance of the RTD. All three leads of a 3-wire RTD typically have the same length and, thus, the same lead resistance. Also, IDAC1 and IDAC2 have the same value. Taking the lead resistance into account, use Equation 17 to calculate the differential voltage (VIN) across the ADC inputs (AIN0 and AIN1):
Equation 17 reduces to Equation 18 when RLEAD1 = RLEAD2 and IIDAC1 = IIDAC2:
In other words, the measurement error resulting from the voltage drop across the RTD lead resistance is compensated, as long as the lead resistance values and the IDAC values are well matched.
A first-order differential and common-mode RC filter (RF1, RF2, CDIF1, CCM1, and CCM2) is placed on the ADC inputs, as well as on the reference inputs (RF3, RF4, CDIF2, CCM3, and CCM4). The same guidelines for designing the input filter apply as described in the K-Type Thermocouple Measurement section. Match the corner frequencies of the input and reference filter for best performance. For more detailed information on matching the input and reference filter, see the RTD Ratiometric Measurements and Filtering Using the ADS1148 and ADS1248 application report.
The reference resistor RREF not only serves to generate the reference voltage for the device, but also sets the voltages at the leads of the RTD to within the specified absolute input voltage range of the PGA.
When designing the circuit, care must also be taken to meet the compliance voltage requirement of the IDACs. The IDACs require that the maximum voltage drop developed across the current path to AVSS be equal to or less than AVDD – 0.9 V in order to operate accurately. This requirement means that Equation 19 must be met at all times.
The device also offers the possibility to route the IDACs to the same inputs used for measurement. If the filter resistor values RF1 and RF2 in Figure 79 are small enough and well matched, then IDAC1 can be routed to AIN1 and IDAC2 to AIN0. In this manner, even two 3-wire RTDs sharing the same reference resistor can be measured with a single device.
As stated in Table 26, this design example discusses the implementation of a 3-wire Pt100 measurement to be used to measure temperatures ranging from –200°C to +850°C. The excitation current for the Pt100 is chosen as IIDAC1 = 500 µA, which means a combined current of 1 mA is flowing through the reference resistor, RREF. As mentioned previously, besides creating the reference voltage for the ADS122U04, the voltage across RREF also sets the absolute input voltages for the RTD measurement. In general, choose the largest reference voltage possible that maintains the compliance voltage of the IDACs and meets the absolute input voltage requirement of the PGA. Setting the common-mode voltage at or near half the analog supply (in this case 3.3 V / 2 = 1.65 V) in most cases satisfies the absolute input voltage requirements of the PGA. Equation 20 is then used to calculate the value for RREF:
The stability of RREF is critical to achieve good measurement accuracy over temperature and time. Choosing a reference resistor with a temperature coefficient of ±10 ppm/°C or better is advisable. If a 1.65-kΩ value is not readily available, another value near 1.65 kΩ (such as 1.62 kΩ or 1.69 kΩ) can certainly be used as well.
As a last step, the PGA gain must be selected in order to match the maximum input signal to the FSR of the ADC. The resistance of a Pt100 increases with temperature. Therefore, the maximum voltage to be measured (VINMAX) occurs at the positive temperature extreme. At 850°C, a Pt100 has an equivalent resistance of approximately 391 Ω as per the NIST tables. The voltage across the Pt100 equates to Equation 21:
The maximum gain that can be applied when using a 1.65-V reference is then calculated as (1.65 V / 195.5 mV) = 8.4. The next smaller PGA gain setting available in the ADS122U04 is 8. At a gain of 8, the ADS122U04 offers an FSR value as described in Equation 22:
This range allows for margin with respect to initial accuracy and drift of the IDACs and reference resistor.
After selecting the values for the IDACs, RREF, and PGA gain, make sure to double check that the settings meet the absolute input voltage requirements of the PGA and the compliance voltage of the IDACs. To determine the true absolute input voltages at the ADC inputs (AIN0 and AIN1), the lead resistance must be taken into account as well.
The smallest absolute input voltage occurs on AIN0 at the lowest measurement temperature (–200°C) with RLEADx = 0 Ω, and is equal to VREF = 1.65 V.
The minimum absolute input voltage must not exceed the limit set in Equation 7 to meet Equation 23:
The restriction is satisfied with VAIN0 = 1.65 V.
The largest absolute input voltage (calculated using Equation 24 and Equation 25) occurs on AIN1 at the highest measurement temperature (850°C).
VAIN1 (MAX) meets the requirement given by Equation 7 and equates to Equation 26 in this design:
The restriction on the compliance voltage (AVDD – 0.9 V = 3.3 V – 0.9 V = 2.4 V) of IDAC1 is met as well.
Table 27 shows the register settings for this design.
REGISTER | SETTING | DESCRIPTION |
---|---|---|
00h | 36h | AINP = AIN1, AINN = AIN0, gain = 8, PGA enabled |
01h | 0Ah | DR = 20 SPS, normal mode, continuous conversion mode, external reference |
02h | 55h | Conversion data counter disabled, data integrity disabled, burnout current sources disabled, IDAC = 500 µA |
03h | 70h | IDAC1 = AIN2, IDAC2 = AIN3, manual data read mode |
04h | 48h | GPIO2/DRDY pin configured as a DRDY output |