SBAS752B May 2017 – October 2018 ADS122U04
PRODUCTION DATA.
Reset the ADC by using the RESET command (06h or 07h). After the RESET command is latched, a delay time of td(RSTX) is required before sending the first serial interface command or starting a conversion; see the UART Timing Requirements table for reset timing information. The exact time that a command is latched in relation to the rising edge of the stop bit depends on the baud rate; see the Command Latching section for details about command latch timing.