SBAS937B September 2018 – December 2018 ADS1278-SP
PRODUCTION DATA.
This input is used when multiple ADS1278-SPs are to be daisy-chained together. The DOUT1 pin of the first device connects to the DIN pin of the next, etc. It can be used with either the SPI or Frame-Sync formats. Data are shifted in on the falling edge of SCLK. When using only one ADS1278-SP, tie DIN low. See the Daisy-Chaining section for more information.