SBAS937B September 2018 – December 2018 ADS1278-SP
PRODUCTION DATA.
In the SPI format, this pin functions as the DRDY output. It goes low when data are ready for retrieval and then returns high on the falling edge of the first subsequent SCLK. If data are not retrieved (that is, SCLK is held low), DRDY pulses high just before the next conversion data are ready, as shown in Figure 72. The new data are loaded within one CLK cycle before DRDY goes low. All data must be shifted out before this time to avoid being overwritten.