SBAS946C April 2021 – September 2022 ADS127L11
PRODUCTION DATA
Spurious-free dynamic range (SFDR) is the ratio of the rms value of a single-tone ac input to the highest spurious signal in the ADC frequency spectrum. SFDR measurement includes harmonics of the original signal. For the SFDR measurement, a –0.2-dBFS, 1-kHz input signal with VCM equal to the mid-supply voltage is applied. As shown in Equation 11, SFDR is the ratio of the rms values of the input signal to the single highest spurious signal, including harmonics of the original signal.
where: