SBAS691B March 2016 – October 2018 ADS1282-SP
PRODUCTION DATA.
DRDY is an output; when it transitions low, this transition indicates new conversion data are ready, as shown in Figure 52. When reading data by the continuous mode, the data must be read within four CLK periods before DRDY goes low again or the data are overwritten with new conversion data. When reading data by the command mode, the read operation can overlap the occurrence of the next DRDY without data corruption.
DRDY resets high on the first falling edge of SCLK. Figure 52 and Figure 53 show the function of DRDY with and without data readback, respectively.
If data are not retrieved (no SCLK provided), DRDY pulses high for four ƒCLK periods during the update time, as shown in Figure 53.