SBAS691B March 2016 – October 2018 ADS1282-SP
PRODUCTION DATA.
This command writes single or multiple register data. The command consists of a two-byte op-code argument followed by the input of register data. The first byte of the op-code contains the starting address and the second byte specifies the number of registers to write – 1.
First command byte: 001r rrrr, where rrrrr is the starting address of the first register.
Second command byte: 000n nnnn, where nnnnn is the number of registers – 1 to write.
Data byte(s): one or more register data bytes, depending on the number of registers specified.
Figure 60 illustrates the WREG command.
A delay of 24 ƒCLK cycles is required between each byte transaction.