SBAS565C January 2014 – August 2019 ADS1283
PRODUCTION DATA.
System calibration of the ADS1283 can be performed without using the calibration commands. This procedure requires the calibration values to be externally calculated and then written to the calibration registers. The steps for this procedure are:
The value written to the FSC registers is calculated by Equation 16 or Equation 17.
DC-signal calibration is shown in Equation 16. The expected output code is based on 31-bit output data.
For ac-signal calibration, use an RMS value of collected data, as shown in Equation 17: