SBAS565C January 2014 – August 2019 ADS1283
PRODUCTION DATA.
The WAKEUP command is used to exit the standby mode. After sending this command, the time for the first data to be ready is illustrated in Figure 48 and Table 16. Sending this command during normal operation has no effect; for example, reading data by the read-data-continuous mode with DIN held low.