SBAS559A May 2022 – December 2022 ADS1285
PRODUCTION DATA
The ADC is synchronized by the SYNC pin or by the SYNC command, resulting in restart of the digital filter cycle. Synchronization by the pin occurs on the next rising edge of CLK after SYNC is taken high on the falling edge of CLK. Synchronization by the SYNC command occurs on the rising edge of CLK following the eighth bit of the command.
The following results in loss of synchronization:
There are two synchronization control modes: pulse sync and continuous sync. The synchronization mode is programmed by the SYNC bit of the ID/SYNC register.