SBAS778B June 2017 – August 2019 ADS1287
PRODUCTION DATA.
Compared to the linear phase filter, the minimum phase filter provides a shorter delay from the arrival of an input event to the event appearing in the data output. As shown in Figure 55, the relationship (phase) is not constant versus frequency. Table 11 shows that the filter phase is selected by the PHS bit.
PHS REGISTER BIT | FILTER PHASE |
---|---|
0 | Linear |
1 | Minimum |