SBAS778B June 2017 – August 2019 ADS1287
PRODUCTION DATA.
The RESET command resets the ADC. RESET sets the registers back to default, restarts the conversion process, and engages read-data-continuous mode. The RESET command is functionally equivalent to using the RESET pin, however toggle the CS pin prior to the RESET command to ensure that the serial interface is reset. See Figure 5 for the RESET command timing.