SNAS602C FEBRUARY 2013 – December 2014 ADS1293
PRODUCTION DATA.
TI recommends placing a 0.1-µF ceramic bypass capacitor from VDD to ground as close as possible to the pin. An electrolytic or tantalum capacitor of value larger than 1 µF is recommeded as a bulk capacitor. The bulk capacitor does not need to be in close proximity to the device and could be close to the voltage source terminals or at the output of the voltage regulator. The same recommendations apply for the VDDIO pin.
The CVREF pin requires a 1-µF bypass capacitor-to-ground; this capacitor should have a low ESR and should be placed as close as possible to the pin. The RLDREF pin requires a 0.1-µF ceramic bypass capacitor-to-ground; this capacitor should be placed as close as possible to the pin.