7 |
Reserved |
R |
0h |
Reserved.
Always read 0. |
6 |
F_OPC |
R |
0h |
Command fault.
This bit indicates that a received command is not recognized as valid and the command is ignored. This bit auto-clears on a STAT_1 data transfer, unless the condition remains.
When in a locked state, this bit is set if any command other than LOCK, UNLOCK, NULL, or RREGS is written to the device.
0 : No fault has occurred
1 : Possible invalid command is ignored |
5 |
F_SPI |
R |
0h |
SPI fault.
This bit indicates that one of the status bits in the STAT_S register is set. Read the STAT_S register to clear the bit.
0 : No fault has occurred
1 : A bit in the STAT_S register is set high |
4 |
F_ADCIN |
R |
0h |
ADC input fault.
This bit indicates that one of the ADC input fault detection bits in the STAT_P or STAT_N register is set. Read the STAT_P and STAT_N registers to clear the bit.
0 : No fault has occurred
1 : A bit in the STAT_P or STAT_N register is set high |
3 |
F_WDT |
R |
0h |
Watchdog timer timeout.
This bit indicates if the watchdog timer times out before a new data frame transfer occurs.
0 : No fault has occurred
1 : Timer has run out (resets following register read back) |
2 |
F_RESYNC |
R |
0h |
Resynchronization fault.
This bit is set whenever the signal path is momentarily reset resulting from a DRDY synchronization event. This fault is only possible in synchronous slave mode.
0 : Devices are in sync
1 : Signal path is momentarily reset to maintain synchronization |
1 |
F_DRDY |
R |
0h |
Data ready fault.
This bit is set if data shifted out from the previous result are not complete by the time new ADC data are ready. This bit auto-clears on a STAT_1 transfer, unless the condition remains.
0 : Data read back complete before new data update
1 : New data update during DOUT data transmission |
0 |
F_CHECK |
R |
0h |
DIN check fault.
This bit is set if either of the following conditions are detected:
- Uncorrectable Hamming error correction state is determined for any DIN word transfer when Hamming code is enabled.
- CRC check word on DIN fails. The input command that triggered this error is ignored.
This bit auto-clears on a STAT_S transfer, unless the condition remains.
0 : No error in DIN transmission
1 : DIN transmission error |