SBAS706D April 2015 – April 2019 ADS54J60
PRODUCTION DATA.
A SYSREF pulse is required by the ADS54J60 to reset internal counters. If SYSREF is not present, as can be the case in subclass 0 or 2, this pulse can be done by doing the following register writes shown in Table 5.
ADDRESS (Hex) | DATA (Hex) | COMMENT |
---|---|---|
0-011h | 80h | Set the master page |
0-054h | 80h | Enable manual SYSREF |
0-053h | 01h | Set SYSREF high |
0-053h | 00h | Set SYSREF low |
0-053h | 01h | Set SYSREF high |
0-053h | 00h | Set SYSREF low |