SBAS976A May 2019 – May 2020 ADS7138
PRODUCTION DATA.
To write a single register from the device, as shown in Figure 35, the I2C master must provide an I2C command with four frames. The register address is the address of the register that must be written and the register data is the value that must be written. Table 12 lists the opcodes for different commands. To end the register write command, the master must provide a STOP or a RESTART condition in the I2C frame.
NOTE:
S = start, Sr = repeated start, and P = stop.