SBAS761A February 2020 – February 2020 ADS8355
PRODUCTION DATA.
The full-scale range (FSR) supported at the analog inputs of the device is programmable with the RANGE_SEL bit of the INPUT_CONFIG register. The RANGE_SEL bit has a default value of low. This bit is common for both ADCs (ADC_A and ADC_B). Equation 1 and Equation 2 give the FSR.
VREF_A and VREF_B are the reference voltages going to ADC_A and ADC_B, respectively (as described in the Reference section).
When operating with internal reference mode, the maximum dynamic range of the ADC can be used by programming the appropriate setting for the INPUT_CONFIG and REFDAC_x registers.
Ensure that the ADC analog supply (AVDD) meets the criteria defined in Equation 3 and Equation 4 when the RANGE_SEL bit is set to 1.