SBASAY5 June 2024 ADS8681W
PRODUCTION DATA
The device features an active-high alarm output on the ALARM/SDO-1/GPO pin, provided that the pin is configured for alarm functionality. To enable the ALARM output on the multifunction pin, set the SDO1_CONFIG[1:0] bits of the SDO_CTL_REG register to 01b.
The device features two types of alarm functions: an input alarm and an AVDD alarm.
When the alarm functionality is turned on, both the input and AVDD alarm functions are enabled by default. These alarm functions are selectively disabled by programming the IN_AL_DIS and VDD_AL_DIS bits (respectively) of the RST_PWRCTL_REG register.
Each alarm (input or AVDD) has two associated types of alarm flags: the active alarm flag and the tripped alarm flag. All alarm flags are read in the ALARM_REG register. Both flags are set when the associated alarm is triggered. The active alarm is cleared at the end of the current ADC conversion (and set again if the alarm condition persists). However, the tripped flag is cleared only after ALARM_REG is read.
The ALARM output flags are updated internally at the end of every conversion. These output flags are read during any data frame that the user initiates by bringing the CONVST/CS signal to a low level.
Read the ALARM output flags in three different ways. Read these flags with the ALARM output pin, by reading the internal ALARM registers, or by appending the ALARM flags to the data output.
Figure 6-16 depicts a functional block diagram for the device alarm functionality.