SBAS905C November 2019 – July 2020 ADS8686S
PRODUCTION DATA
The SER/BYTE/PAR is a digital input pin that selects the digital interface option for device communication along with the DB9/BYTESEL pin. If the SER/BYTE/PAR pin is set to logic low at full reset, the parallel interface is selected. If the SER/BYTE/PAR pin is set to logic high at full reset, the serial or byte interface is selected based on the status of the DB9/BYTESEL pin. See the Section 7.5 section for further details.