SBAS650C May 2014 – April 2021 AFE4403
PRODUCTION DATA
The lowest power consumption mode of the AFE4403 corresponds to the following settings:
With the above settings, the currents taken from the supplies are as shown in Table 10-1. The LED driver current is with zero LED current setting.
SUPPLY | VOLTAGE (V) | CURRENT (µA) |
---|---|---|
RX_ANA | 2 | 490 |
RX_DIG | 2 | 155 |
TX_CTRL_SUP | 3 | 15 |
LED_DRV_SUP | 3 | 55 |
Enabling the crystal (XTALDIS = 0) leads to an additional power consumption that can be estimated to be approximately equal to (2 × Csh + 0.5 × C1 + 0.5 × C2) × 0.4 × fXTAL, where Csh is the effective shunt capacitance of the crystal, C1 and C2 are the capacitances from the XIN and XOUT pins to ground, and fXTAL is the frequency of the crystal.
Removing the CLKOUT tri-state leads to an additional power consumption of approximately CLOAD × VSUP × f, where VSUP is the supply voltage of RX_DIG in volts, f = 4 MHz, CLOAD = the capacitive load on the CLKOUT pin + 2 pF.
The power consumption can be reduced significantly by using the dynamic power-down mode. An illustration of this mode is shown in Table 10-2, where:
SUPPLY | VOLTAGE (V) | CURRENT (µA) |
---|---|---|
RX_ANA | 2 | 150 |
RX_DIG | 2 | 155 |
TX_CTRL_SUP | 3 | 5 |
LED_DRV_SUP | 3 | 5 |