SBAS650C May 2014 – April 2021 AFE4403
PRODUCTION DATA
The receiver provides digital samples corresponding to ambient duration. The host processor (external to the AFE) can use these ambient values to estimate the amount of ambient light leakage. The processor must then set the value of the ambient cancellation DAC using the SPI, as shown in Figure 8-4.
Using the set value, the ambient cancellation stage subtracts the ambient component and gains up only the pleth component of the received signal; see Figure 8-5. The amplifier gain is programmable to 0 dB, 3.5 dB, 6 dB,
9.5 dB, and 12 dB.
The differential output of the second stage is VDIFF, as given by Equation 3:
where:
RG values with various gain settings are listed in Table 8-1.
GAIN | RG(kΩ) |
---|---|
0 (x1) | 100 |
3.5 (x1.5) | 150 |
6 (x2) | 200 |
9.5 (x3) | 300 |
12 (x4) | 400 |