SBASB81 December 2024 AFE5401-EP
PRODUCTION DATA
All analog inputs must be differentially and symmetrically routed to the differential input pins of the device for best performance. CMOS outputs traces should be kept as short as possible to reduce the trace capacitance that loads the CMOS output buffers. Multiple ground vias can be added around the CMOS output data traces, especially when the traces are routed on more than one layer. TI recommends matching the lengths of the output data traces (D[11:0]) to reduce the skew across data bits.
Switching noise (caused by CMOS output data transitions) can couple into the analog inputs and degrade SNR. This condition is particularly of concern because of the high gain present in the analog input channel. Digital outputs coupling back to analog inputs can be minimized by proper separation of analog and digital areas in the board layout. Figure 8-10 illustrates an example layout where the analog and digital portions are routed separately. This example also uses splits in the ground plane to minimize digital currents from looping into analog areas. At the same time, note that the analog and digital grounds are shorted below the device. A single ground plane is sufficient to give good performance, provided the analog, digital, and clock sections of the board are cleanly partitioned.
The device package consists of an exposed pad. In addition to providing a path for heat dissipation, the pad is also internally connected to the analog ground. Therefore, the exposed pad must be soldered to the ground plane for best thermal and electrical performance. For detailed information, see application notes QFN Layout Guidelines and QFN/SON PCB Attachment. Figure 8-10 and Figure 8-11 illustrate the layout diagrams taken from the AFE5401-Q1 EVM User's Guide.