SBASAX1 August 2024 AMC0106M25
ADVANCE INFORMATION
Figure 6-2 conceptualizes the second-order, switched-capacitor, feed-forward ΔΣ modulator implemented in the AMC0106M25. The output V5 of the 1-bit, digital-to-analog converter (DAC) is subtracted from the input voltage VIN = (VINN – VINP). This subtraction provides an analog voltage V1 at the input of the first integrator stage. The output of the first integrator feeds the input of the second integrator stage. The result is an output voltage V3 that is summed with the input signal VIN and the output of the first integrator V2. Depending on the polarity of the resulting voltage V4, the output of the comparator is changed. In this case, the 1-bit DAC responds on the next clock pulse by changing the associated analog output voltage V5. Thus, causing the integrators to progress in the opposite direction and forcing the integrator output value to track the average value of the input.