SBASAZ5 October 2024 AMC0386-Q1
ADVANCE INFORMATION
Refer to the PDF data sheet for device specific package drawings
As shown in Figure 6-5, the device provides a constant bitstream of logic 0's at the output if the high-side supply is missing. DOUT is permanently low when the high-side supply is missing. A one is not generated every 128 clock pulses, which differentiates this condition from a valid negative fullscale input. This feature helps identify high-side power-supply problems on the board.