SBAS837B August 2018 – April 2020 AMC1035
PRODUCTION DATA.
If a full-scale input signal is applied to the AMC1035 (that is, |VIN| ≥ |VClipping|), the device generates a single one or zero every 128 bits at DOUT, as shown in Figure 43, depending on the actual polarity of the signal being sensed. This feature is also supported with Manchester-coded output and allows full-scale and invalid input signals to be identified as described in the Fail-Safe Output section and can be used for advanced system-level diagnostics.