SBAS427D February 2008 – June 2024 AMC1203
PRODUCTION DATA
The shunt resistor (RSHUNT) value is determined by the device linear input voltage range (±280mV) and the desired ±5.6A linear current sensing range. RSHUNT is calculated as 280mV / 5.6A = 50mΩ. The peak power dissipated in the shunt resistor is RSHUNT × IPEAK2 = 50mΩ × (5.6A)2 = 1.57W. For a linear response, operate the shunt resistor at no more than 2/3 of the rated power. Therefore, select a shunt resistor with a nominal power rating of approximately 2W.
Select a lower shunt resistor value if overcurrent transients are expected in the system that exceed the linear input voltage range of the AMC1203. Alternatively, the voltage drop across the shunt is allowed to exceed the linear input voltage range of the AMC1203. Outside the linear range, however, the output accuracy and noise performance degrades. Regardless, make sure the maximum overcurrent does not cause a voltage drop across the shunt that exceeds the clipping voltage of the AMC1203. That is, make sure |VSHUNT| ≤ |VClipping|.