SBASA57 September 2023 AMC131M01
PRODUCTION DATA
The AMC131M01 has a dedicated input multiplexer. The multiplexer controls which signals are routed to the ADC. Configure the input multiplexer using the MUX0[1:0] bits in the CH0_CFG register. The input multiplexer allows the following inputs to be connected to the ADC: