SBASA56 September 2023 AMC131M02
PRODUCTION DATA
Figure 9-5 illustrates phase A of a three-phase energy meter. The other AMC131M02 devices that monitor phases B and C are connected in a similar way. The phase A current, ISHUNT, is sensed with a shunt resistor (RSHUNT) using channel 0 of the ADC (AIN0N, AIN0P). One terminal of the shunt becomes the isolated ground ISO_GND of the circuit and is connected to the ground pin HGND (pin 5) of the isolated side of the AMC131M02. The phase A to neutral voltage VPHASEA is sensed with a resistor divider connected to channel 1, and the AIN1N pin is also connected to the ISO_GND node. The high side of the resistor divider is connected to the neutral line, the mid-point of the resistor divider is connected to the positive ADC input AIN1P, and the low side of the resistor divider (which is sensing the ISO_GND node) is connected to the negative input AIN1N of channel 1; therefore, the negative phase voltage is measured at channel 1. Thus, voltages measured by channel 1 of the AMC131M02 are opposite in sign to the phase voltage VPHASEA and the phase current ISHUNT, which is a classic approach in single-phase and poly-phase metering.
The selection of the shunt resistor value is made based on the manufacturer and current range required for energy measurements. The voltage divider resistors for the voltage channel are selected to make sure the mains voltage is divided down to adhere to the normal input voltage ranges of the AMC131M02.
In this design, the AMC131M02 interacts with an MCU in the following manner: