SBASAJ7A June 2022 – August 2022
PRODUCTION DATA
The AMC22C11-Q1 is operational when the power supplies VDD1 and VDD2 are applied, as specified in the Section 6.3 table.
The voltage on the REF pin affects the threshold of the comparator. For reference voltages below the VMSEL threshold, the comparator operates in low-hysteresis mode. For reference voltages above the VMSEL threshold, the comparator operates in high-hysteresis mode as described in the Section 7.3.2 section.
The device has two output operating modes that are selected based on the LATCH input pin setting: transparent mode and latch mode. These modes affect how the OUT pin responds to the changing input signal conditions. See the Section 7.3.4 section for details.