SBASAJ6B April 2022 – December 2024 AMC22C11
PRODUCTION DATA
The AMC22C11 provides an open-drain output with an optional latching function. The output is actively pulled low when VIN exceeds the threshold value defined by the voltage on the REF pin, see Figure 6-1.
The open-drain output is diode-connected to the VDD2 supply (see the Functional Block Diagram), meaning that the output cannot be pulled more than 500mV above the VDD2 supply before significant current begins to flow into the OUT pin. In particular, the open-drain output is clamped to one diode voltage above ground if VDD2 is at the GND2 level. This behavior is indicated by the gray shadings in Figure 6-5 through Figure 6-10.
On a system level, the CMTI performance of an open-drain signal line depends on the value of the pullup resistor. During a common-mode transient event with a high slew rate (high dV/dt), the open-drain signal line can be pulled low because of parasitic capacitive coupling between the high side and the low side of the printed circuit board (PCB). The effect of the parasitic coupling on the signal level is a function of the pullup strength and a lower value pullup resistor results in better CMTI performance. The AMC22C11 is characterized by a relatively weak pullup resistor value of 10kΩ to make sure that the specified CMTI performance is met in a typical application with a 4.7kΩ or lower pullup resistor.