SBASAJ9B June 2022 – December 2024 AMC22C12-Q1
PRODUCTION DATA
PIN | TYPE | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
1 | VDD1 | High-side power | High-side power supply(1) |
2 | IN | Analog input | Analog input pin to the window comparator |
3 | REF | Analog input | Reference pin that defines the trip threshold. The voltage on this pin also affects the hysteresis of comparator Cmp0, as explained in the Reference Input section. This pin is internally connected to a 100μA current source. Connect a resistor from REF to GND1 to define the trip threshold, and a capacitor from REF to GND1 to filter the reference voltage. For best transient noise immunity, place the capacitor as closely to the pin as possible. This pin can also be driven by an external voltage source. |
4 | GND1 | High-side ground | High-side ground |
5 | GND2 | Low-side ground | Low-side ground |
6 | OUT | Digital output | Open-drain output of the window comparator. Connect to an external pullup resistor. |
7 | LATCH | Digital input | Digital input to select latch mode (high) or transparent mode (low) of the open-drain output. Do not leave the input pin unconnected (floating). Connect to GND2 when not used. |
8 | VDD2 | Low-side power | Low-side power supply(1) |