SBASAJ9A June 2022 – August 2022 AMC22C12-Q1
PRODUCTION DATA
PIN | TYPE | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
1 | VDD1 | High-side power | High-side power supply.(1) |
2 | IN | Analog input | Common analog input pin for window comparator 1 and 2. |
3 | REF | Analog input | Reference pin that defines the trip threshold for window comparator 1. The voltage on this pin also affects the hysteresis of comparator Cmp0 as explained in the Section 7.3.2 section. This pin is internally connected to a 100-μA current source. Connect a resistor from REF to GND1 to define the trip threshold, and a capacitor from REF to GND1 to filter the reference voltage. For best transient noise immunity, place the capacitor as closely to the pin as possible. This pin can also be driven by an external voltage source. |
4 | GND1 | High-side ground | High-side ground. |
5 | GND2 | Low-side ground | Low-side ground. |
6 | OUT1 | Digital output | Open-drain output of window comparator 1. Connect to an external pullup resistor or leave unconnected (floating) when not used. |
7 | OUT2 | Digital output | Open-drain output of window comparator 2. Connect to an external pullup resistor or leave unconnected (floating) when not used. |
8 | VDD2 | Low-side power | Low-side power supply.(1) |