SBAS945A February 2022 – July 2022 AMC23C14
PRODUCTION DATA
The AMC23C14 is operational when the power supplies VDD1 and VDD2 are applied, as specified in the Section 6.3 table.
The four comparators on the high-side (Cmp0 to Cmp3) function as two independent window comparators when the voltage on the REF pin is below the VMSEL threshold. If the voltage on the REF pin exceeds the VMSEL threshold, the negative comparators (Cmp1 and Cmp3) are disabled, and Cmp0 and Cmp2 function as two independent positive comparators, as described in the Section 7.3.2 section.