SBASAQ0 March 2023 AMC23C15-Q1
PRODUCTION DATA
The AMC23C15-Q1 has a single input that drives both window comparators. Window comparator 1 has an adjustable threshold and window comparator 2 has a fixed threshold.
The positive comparators trip when the input voltage (VIN) rises above the respective VIT+ threshold that is defined as the reference value plus the internal hysteresis voltage (for example, 64 mV for the fixed-threshold comparator). The positive comparators release when VIN drops below the respective VIT– threshold that equals the reference value (for example, 60 mV for the fixed-threshold comparator). The negative comparators trip when VIN drops below the respective VIT– threshold that is defined as the negative reference value minus the internal hysteresis voltage (for example, –64 mV for the fixed-threshold comparator). The negative comparators release when VIN rises above the respective VIT+ threshold that equals the negative reference value (for example –60 mV for the fixed-threshold comparator).
The difference between VIT+ and VIT– is referred to as the comparator hysteresis and is 4 mV for reference voltages below 450 mV. The integrated hysteresis makes the AMC23C15-Q1 less sensitive to input noise and provides stable operation in noisy environments without having to add external positive feedback to create hysteresis. The hysteresis of Cmp0 increases to 25 mV for reference values (VREF) greater than 600 mV. See the Reference InputAnalog InputReference InputReference Input description for more details.
Figure 7-1 shows a timing diagram of the relationship between hysteresis and switching thresholds.