SBASAQ0 March 2023 AMC23C15-Q1
PRODUCTION DATA
Both open-drain outputs power up in a high-impedance (Hi-Z) state when the low-side supply (VDD2) turns on. After power-up, if the high-side is not functional yet, both outputs are actively pulled low. As shown in Figure 7-5, this condition happens after the low-side start-up time plus the high-side fault detection delay time (tLS,STA + tHS,FLT). Similarly, if the high-side supply drops below the undervoltage threshold (VDD1UV), as described in Figure 7-8, for more than the high-side fault detection delay time during normal operation, both outputs are pulled low. This delay allows the system to shut down reliably when the high-side supply is missing.
Communication start between the high-side and low-side of the comparator is delayed by the high-side blanking time (tHS,BLK, a time constant implemented on the high-voltage side) to allow the internal 60-mV reference and the voltage on the REF pin to settle, and to avoid unintentional switching of the comparator outputs during power-up.
Figure 7-5 through Figure 7-10 depict typical power-up and power-down scenarios.
In Figure 7-5, the low-side supply (VDD2) turns on but the high-side supply (VDD1) remains off. Both outputs power up in the default Hi-Z state. After tHS,FLT, both outputs are pulled low indicating a no-power fault on the high-side.
In Figure 7-6, the high-side supply (VDD1) turns on long after the low-side supply (VDD2) turns on. Both outputs are initially in an active-low state, see Figure 7-5. After the high-side supply is enabled, there is a duration of tHS, STA + tHS,BLK before the device assumes normal operation and both outputs reflect the current state of the window comparators.
In Figure 7-7, the low-side supply (VDD2) turns on, followed by the high-side supply (VDD1) with only a short delay. Both outputs are initially in a Hi-Z state. The high-side fault detection delay (tHS,FLT) is shorter than the high-side blanking time (tHS,BLK), and therefore both outputs are pulled low after tHS, FLT, indicating that the high-side is not operational yet. After the high-side blanking time (tHS,BLK) elapses, the device assumes normal operation and both outputs reflect the current state of the window comparators.
In Figure 7-8, the high-side supply (VDD1) turns off, followed by the low-side supply (VDD2). After the high-side fault detection delay time (tHS,FLT), both outputs are actively pulled low. As soon as VDD2 drops below the VDD2UV threshold, both outputs enter a Hi-Z state.
In Figure 7-9, the low-side supply (VDD2) turns on after the high-side is fully powered up (the delay between VDD1 and VDD2 is greater than (tHS,STA + tHS,BLK)). Both outputs start in a Hi-Z state. After the low-side start-up time (tLS,STA), the device enters normal operation.
In Figure 7-10, the low-side supply (VDD2) turns off, followed by the high-side supply (VDD1). As soon as VDD2 drops below the VDD2UV threshold, both outputs enter a Hi-Z state.