SBASAP9 March 2023 AMC23C15
PRODUCTION DATA
The AMC23C15 is operational when the power supplies VDD1 and VDD2 are applied, as specified in the Recommended Operating Conditions table.
The four comparators on the high-side (Cmp0 to Cmp3) function as two independent window comparators when the voltage on the REF pin is below the VMSEL threshold. If the voltage on the REF pin exceeds the VMSEL threshold, the negative comparators (Cmp1 and Cmp3) are disabled, and Cmp0 and Cmp2 function as two independent positive comparators, as described in the Reference Input section.