ADC_0 |
47 |
I |
Bipolar analog inputs. These pins are typically used to monitor the DAC group-C outputs. The input range of these channels is –12.5 to 12.5 V. |
ADC_1 |
46 |
I |
ADC_2 |
45 |
I |
ADC_3 |
44 |
I |
ADC_4 |
43 |
I |
Bipolar analog inputs. These pins are typically used to monitor the DAC group-D outputs. The input range of these channels is –12.5 to 12.5 V. |
ADC_5 |
42 |
I |
ADC_6 |
41 |
I |
ADC_7 |
40 |
I |
ADC_8 |
34 |
I |
Bipolar analog inputs. These pins are typically used to monitor the DAC group-B outputs. The input range of these channels is –12.5 to 12.5 V. |
ADC_9 |
33 |
I |
ADC_10 |
32 |
I |
ADC_11 |
31 |
I |
ADC_12 |
30 |
I |
Bipolar analog inputs. These pins are typically used to monitor the DAC group-A outputs. The input range of these channels is –12.5 to 12.5 V. |
ADC_13 |
29 |
I |
ADC_14 |
28 |
I |
ADC_15 |
27 |
I |
AGND1 |
21 |
I |
Analog ground. These pins are the ground reference point for all analog circuitry on the device. Connect the AGND1, AGND2, and AGND3 pins to the same potential (AGND). Ideally, the analog and digital grounds should be at the same potential (GND) and must not differ by more than ±0.3 V. |
AGND2 |
48 |
I |
AGND3 |
56 |
I |
AVCC_AB |
20 |
I |
Positive analog power for DAC groups A and B. The AVCC_AB and AVCC_CD pins must be connected to the same potential (AVCC). |
AVCC_CD |
57 |
I |
Positive analog power for DAC groups C and D. The AVCC_AB and AVCC_CD pins must be connected to the same potential (AVCC). |
AVDD |
50 |
I |
Analog supply voltage (4.7 V to 5.5 V). This pin must have the same value as the DVDD pin. |
AVEE |
17 |
I |
Lowest potential in the system. This pin is typically tied to a negative supply voltage but if all DACs are set in a positive output range, this pin can be connected to the analog ground. This pin also acts as the negative analog supply for DAC group A. This pin sets the power-on-reset and clamp voltage values for the DAC group A. |
AVSSB |
24 |
I |
Negative analog supply for DAC group B. This pin sets the power-on-reset and clamp voltage values for the DAC group B. This pin is typically tied to the AVEE pin for the negative output ranges or AGND for the positive output ranges. |
AVSSC |
53 |
I |
Negative analog supply for DAC group C. This pin sets the power-on-reset and clamp voltage values for the DAC group C. This pin is typically tied to the AVEE pin for the negative output ranges or AGND for the positive output ranges. |
AVSSD |
60 |
I |
Negative analog supply for DAC group D. This pin sets the power-on-reset and clamp voltage values for the DAC group D. This pin is typically tied to the AVEE pin for the negative output ranges or AGND for the positive output ranges. |
CS |
6 |
I |
Active-low serial-data enable. This input is the frame-synchronization signal for the serial data. When this signal goes low, it enables the serial interface input shift register. |
DAC_A0 |
15 |
O |
DAC group A. These DAC channels share the same range and clamp voltage. If any of the other DAC groups is in a negative voltage range, DAC group A should be in a negative voltage range as well. |
DAC_A1 |
16 |
O |
DAC_A2 |
18 |
O |
DAC_A3 |
19 |
O |
DAC_B4 |
22 |
O |
DAC group B. These DAC channels share the same range and clamp voltage. |
DAC_B5 |
23 |
O |
DAC_B6 |
25 |
O |
DAC_B7 |
26 |
O |
DAC_C8 |
51 |
O |
DAC group C. These DAC channels share the same range and clamp voltage. |
DAC_C9 |
52 |
O |
DAC_C10 |
54 |
O |
DAC_C11 |
55 |
O |
DAC_D12 |
58 |
O |
DAC group D. These DAC channels share the same range and clamp voltage. |
DAC_D13 |
59 |
O |
DAC_D14 |
61 |
O |
DAC_D15 |
62 |
O |
DGND |
64 |
I |
Digital ground. This pin is the ground reference point for all digital circuitry on the device. Ideally, the analog and digital grounds should be at the same potential (GND) and must not differ by more than ±0.3 V. |
DVDD |
63 |
I |
Digital supply voltage (4.7 V to 5.5 V). This pin must have the same value as the AVDD pin. |
GPIO0/ALARMIN |
7 |
I/O |
General-purpose digital I/O 0 (default). This pin is a bidirectional digital input/output (I/O) with an internal 48-kΩ pullup resistor to the IOVDD pin. Alternatively the pin can be set to operate as the digital input ALARMIN which is an active-low alarm-control signal. If unused this pin can be left floating. |
GPIO0/ALARMOUT |
8 |
I/O |
General purpose digital I/O 1 (default). This pin is a bidirectional digital I/O with an internal 48-kΩ pullup resistor to the IOVDD pin. Alternatively the pin can be set to operate as ALARMOUT which is an open drain global alarm output. This pin goes low (active) when an alarm event is detected. If unused this pin can be left floating. |
GPIO2/ADCTRIG |
9 |
I/O |
General purpose digital I/O 2 (default). This pin is a bidirectional digital I/O with internal 48-kΩ pullup resistor to the IOVDD pin. Alternatively the pin can be set to operate as ADCTRIG which is an active-low external conversion trigger. The falling edge of this pin begins the sampling and conversion of the ADC. If unused this pin can be left floating. |
GPIO3/DAV |
10 |
I/O |
General purpose digital I/O 3 (default). This pin is a bidirectional digital I/O with internal 48-kΩ pullup resistor to the IOVDD pin. Alternatively the pin can be set to operate as DAV which is an active-low data-available indicator output. In direct mode, the DAV pin goes low (active) when the conversion ends. In auto mode, a 1-µs pulse (active low) appears on this pin when a conversion cycle finishes. The DAV pin remains high when deactivated. If unused this pin can be left floating. |
GPIO4 |
11 |
I/O |
General purpose digital I/O. These pins are bidirectional digital I/Os with an internal 48-kΩ pullup resistor to the IOVDD pin. If unused these pins can be left floating. |
GPIO5 |
12 |
I/O |
GPIO6 |
13 |
I/O |
GPIO7 |
14 |
I/O |
IOVDD |
1 |
I |
I/O supply voltage (1.8 V to 5.5 V). This pin sets the I/O operating voltage and threshold levels. The voltage on this pin must not be greater than the value of the DVDD pin. |
LV_ADC16 |
39 |
I |
General purpose analog inputs. These channels are used for general monitoring. The input range of these pins is 0 to 2 × Vref. |
LV_ADC17 |
38 |
I |
LV_ADC18 |
37 |
I |
LV_ADC19 |
36 |
I |
LV_ADC20 |
35 |
I |
REF_CMP |
49 |
O |
Internal-reference compensation-capacitor connection. Connect a 4.7-μF capacitor between this pin and the AGND2 pin. |
RESET |
2 |
I |
Active-low reset input. Logic low on this pin causes the device to perform a hardware reset. |
SCLK |
5 |
I |
Serial interface clock. |
SDI |
4 |
I |
Serial-interface data input. Data is clocked into the input shift register on each rising edge of the SCLK pin. |
SDO |
3 |
O |
Serial-interface data output. The SDO pin is in high impedance when the CS pin is high. Data is clocked out of the input shift register on each falling edge of the SCLK pin. |
Thermal Pad |
— |
I |
The thermal pad is located on the bottom-side of the device package. The thermal pad should be tied to the same potential as the AVEE pin or left disconnected. |