SLUSFR2 November 2024 BQ21088
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The device has an internal pulldown on the SYS pin which is enabled in the following cases:
STATE |
NOTES |
---|---|
Shipmode |
Pulldown on SYS is enabled once the device enters the shipmode and after disconnecting the BATFET |
HW_RESET |
Pulldown on SYS is enabled after the BATFET and ILIM FET are disconnected and retained until the autowake timer expires |
SYS_MODE = 11 (SYS pulldown mode) |
Pulldown on SYS is enabled after the BATFET and ILIM FET are disconnected and retained till either an I2C transaction – changing SYS_MODE or a hardware reset – is given or VIN is toggled. |