SLUSFR2 November 2024 BQ21088
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
When a valid input source is connected (VIN > VINDPM and VBAT +VSLEEP < VIN < VIN_OVP), the state of the CHARGE_DISABLE bit and the TS/MR pin determine whether a charge cycle is initiated. When the CHARGE_DISABLE bit is set to disable charging, VHOT < VTS/MR < VCOLD and a valid input source is connected, the battery FET is turned off, preventing any kind of charging of the battery. Note that supplement behavior is independent of the CHARGE_DISABLE bit. The device will be able to charge a battery as long as VIN voltage is higher than the VIN_LOWV threshold. This threshold is present as the VIN can be considered "powergood" with a very low battery voltage or a 0-V battery.
The following figure illustrates a typical charge cycle.