SLUSFR2 November 2024 BQ21088
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The device is capable of hardware reset to completely powercycle the system. This is partcularly useful when a soft reset on the MCU or host fails to work. A hardware reset needs to be possible in all SYS MODES.
There are a few ways a hardware reset occurs. A hardware reset will occur when:
Below is a sequence of events during a hadware reset:
At a time tRESET_WARN before the reset pulldown on SYS occurs, an interrupt occurs to signify a hardware reset is about to occur.