SLUSFR2 November 2024 BQ21088
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The device also offers the option to control SYS through the I2C SYS_MODE bits. These bits can force SYS to be supplied by BAT instead of IN (even if VIN > VBAT + VSLEEP), disconnect SYS from either supply, pull SYS down or leave it floating. The table below shows the device behavior based on SYS_MODE setting:
SYS_MODE | DESCRIPTION | SYS SUPPLY | SYS PULL-DOWN |
---|---|---|---|
00 |
Normal Operation |
IN or BAT |
Off except during HW reset |
01 |
Force BAT power (USB Suspend) |
BAT |
Off except during HW reset |
10 |
SYS Off –Floating |
None |
Off |
11 |
SYS Off – Pulled Down |
None |
On |
SYS_MODE = 00
This is the default state / normal operation of the device. SYS will be powered from IN if VIN > VUVLO, VIN > VBAT + VSLEEP, and VIN < VIN_OVP. SYS will powered by BAT if these conditions are not met. SYS will only be disconnected from IN or BAT and pulled down when a HW Reset occurs or the device goes into Ship mode.
SYS_MODE = 01
When this configuration is set, SYS will be powered by BAT if VBAT > VBUVLO regardless of VIN state. This allows the host to minimize the current draw from the adapter while it is still connected as needed in the system.If SYS_MODE = 01 is set while VBAT < VBUVLO, the SYS_MODE = 01 setting will be ignored and the device will go to SYS_MODE = 00. In the same manner, if the adapter (VIN) is removed and then connected the device will also switch to SYS_MODE=00. This prevents the device from needing a POR in order to restore power to the system thereby allowing battery charging and providing a true USB suspend mode. If SYS_MODE = 01 is set during charging, charging will be stopped and the battery will start to provide power to SYS as needed. The behavior is similar to that when the input adapter is disconnected.
SYS_MODE = 10
When this configuration is set, SYS will be disconnected and left floating. The digital remains on and active. When floating, SYS can only be forced to a voltage up to VBAT level. Toggling VIN(VIN <VINUVLO) will reset the SYS_MODE to 00.
SYS_MODE = 11
When this configuration is set, SYS will be disconnected and pulled down to ground. Toggling VIN will reset the SYS_MODE to 00.